Part Number: DS90UB933-Q1
1.We are using the setup Camera -> UB933 Serializer -> FPD Link -> UB954 Deserializer -> Jacinto 7 Board. In the Imaging folder, we create the separate folder for new camera. In the new camera folder, there is a header file for serializer and deserializer configuration. Below is the iss_serdes_cameraname.h header file for UB933 serializer and UB954 deserializer configuration. Please check and let me know if there is any mistake.
#ifndef _AR0233_SERDES_H_
#define _AR0233_SERDES_H_
/**
7-bit Alias addresses for sensor and serializer
Physical addresses must be programmed in UB96x config
SoC will communicate with the devices using alias adresses
*/
//#define _TEST_PATTERN_ENABLE_
#ifdef _TEST_PATTERN_ENABLE_
#define AR0233_SER_CFG_SIZE (37U)
#else
#define AR0233_SER_CFG_SIZE (6U)
#endif
#define AR0233_I2C_ADDR (0x10U)
I2cParams ub933SerCfg_AR0233[AR0233_SER_CFG_SIZE] = {
{0x1, 0x2, 1000},/////////////////////////////////////////Digital Reset 1 in RESET_CTL Register
{0xE, 0x99, 0x1},/////////////////////////////////////////Enable GPO 2 and GPO 3
{0xD, 0x99, 0x1},/////////////////////////////////////////Enable GPO 0 and GPO 1
{0x05,0x02,0x1},//////////////////////////////////////////Enable 12bit HF mode - Doubt
{0x29,0x00,0x1},///////////////////////////////////////////External oscillator mode
{0xFFFF, 0x00, 0x0} //End of script
};
#define AR0233_DES_CFG_SIZE (13U)
I2cParams ub954DesCfg_AR0233[AR0233_DES_CFG_SIZE] = {
{0x1, 0x2, 1000},
{0x4C, 0x01, 0x1},/////////////////////////////////////////////////////////FPD3_PORT_SEL Register Select Port 0
{0x0C,0x81,0x1}////////////////////////////////////////////////////////////Enable Port 0
{0x58, 0x58, 0x1},/////////////////////////////////////////////////////////BCC_CONFIG (Enable I2C Passthrough)
{0x5C, (SER_0_I2C_ALIAS << 1), 0x10},//////////////////////////////////////Serializer Alias ID
{0x5D, (SENSOR_0_I2C_ALIAS << 1), 0x10},///////////////////////////////////Slave ID
{0x65, (SENSOR_0_I2C_ALIAS << 1), 0x10},//////////////////////////////////////Slave Alias ID
{0x6D,0x7E,0x01},//////////////////////////////////////////////////////////////Coax mode and raw 12 bit mode select
{0x32, 0x21, 0x1},/////////////////////////////////////////////////////////CSI-2 Tx port select
{0x33, 0x03, 0x1},/////////////////////////////////////////////////////////CSI-2 Lane select
{0x21, 0x01, 0x1},/////////////////////////////////////////////////////////Enable round robin forwarding for CSI TX output port
{0x20, 0x20, 0x1},/////////////////////////////////////////////////////////Forwarding enabled for Rx port 0
{0xFFFF, 0x00, 0x0} //End of script
};
I2cParams ub954AR0233DesCSI2Enable[2u] = {
{0x33, 0x03, 0x10},
{0xFFFF, 0x00, 0x0} //End of script
};
I2cParams ub954AR0233DesCSI2Disable[2u] = {
{0x33, 0x00, 0x10},
{0xFFFF, 0x00, 0x0} //End of script
};
#endif /* _AR0233_SERDES_H_ */