Hi,
I am trying to understand the internal oscillator setting when auto-switch is enabled in "PCLK Auto" (bit 1 of 0x03)
If PCLK is not externally present does the internal oscillator default to the OSC Clock Source set in 0x14 or does it set its internal timing based off the configuration settings of horizontal and vertical width, back porch, etc like for pattern generation?
Additionally, what is the range of internal oscillator? It looks like 25MHz - 100MHz.