Part Number: DS90LV018A
Other Parts Discussed in Thread: SN74AUC1G125
Hi There,
We are considering the adoption of "DS90LV018ATMX/NOPB".
Since the system in the second stage is 1.8V, it is necessary to divide the voltage.
Attenuates at 68 Ω/ 75Ω. ( 75Ω / (68Ω+75Ω) * 3.3V ≒ 1.731V )
I want to reduce the load because the frequency is high(100MHz).
Therefore, I want to know the output current driven.
How much drive output current is possible?
Best regards
- satoshi