Part Number: DS90UB954-Q1
Hi, TI engineers.
I am currently building my system with Raspberry Pi 4B, UB954, UB953 and sensor.
The first question is about i2c. Currently I am using TI’s 953 and 954 EVM boards. When I use Raspberry Pi to detect i2c devices, why only the 953, 954 and sensor i2c addresses appear on the bus? Why can't the msp 430 on the board be detected? Maybe msp 430 also exists as a master device? So is there a way to use a MCU similar to msp430 as a slave device?
The second question is about the poc. There may be LED devices on our custom development board, plus the 953 and sensor will have a total power demand of about 3W. I want to transfer all the electrical energy through poc. I also checked the corresponding information.
Below is the corresponding information about capacitors and magnetic beads.
What kind of power supply plan should I make? What is the voltage on the poc? Do I need to change specifications for inductors and magnetic beads?