This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH941AS-Q1: FPDLink initialization fail between DS90UH941AS and DS90UH948

Part Number: DS90UH941AS-Q1

Hi

     we've encountered a problem using DS90UH941AS and DS90UH948.

     the fpdlink is not correctly setup and the link training seems to be a failure.

   

    the hardware connection is like:

SOC---DSI0---DS90UH941AS ------port0--------LCD0

           |

           DSI1----DS90UH941AS ----port0---------LCD1

FOR LCD0:

    The dump of the DS90UH941AS  is as follows:

0x00--0x18 0x01--0x00 0x02--0x00 0x03--0x9a
0x04--0x00 0x05--0x00 0x06--0x58 0x07--0x48
0x08--0xd6 0x09--0x01 0x0a--0x6f 0x0b--0xa2
0x0c--0x07 0x0d--0x30 0x0e--0x31 0x0f--0x01
0x10--0x33 0x11--0x00 0x12--0x00 0x13--0xdf
0x14--0x00 0x15--0x00 0x16--0xfe 0x17--0x1e
0x18--0x7f 0x19--0x7f 0x1a--0x01 0x1b--0x00
0x1c--0x00 0x1d--0x00 0x1e--0x04 0x1f--0x00
0x20--0x83 0x21--0x00 0x22--0x25 0x23--0x00
0x24--0x00 0x25--0x00 0x26--0x00 0x27--0x00
0x28--0x01 0x29--0x20 0x2a--0x20 0x2b--0xa0
0x2c--0x00 0x2d--0x00 0x2e--0xa5 0x2f--0x5a
0x30--0x01 0x31--0x09 0x32--0x80 0x33--0x07
0x34--0x0c 0x35--0x00 0x36--0x00 0x37--0x00
0x38--0x00 0x39--0x00 0x3a--0x00 0x3b--0x00
0x3c--0x00 0x3d--0x00 0x3e--0x81 0x3f--0x02
0x40--0x04 0x41--0x05 0x42--0x54 0x43--0x00
0x44--0x00 0x45--0x00 0x46--0x80 0x47--0x00
0x48--0x00 0x49--0x00 0x4a--0x00 0x4b--0x00
0x4c--0x00 0x4d--0x00 0x4e--0x00 0x4f--0x8c
0x50--0x16 0x51--0x00 0x52--0x00 0x53--0x00
0x54--0x02 0x55--0x10 0x56--0x81 0x57--0x02
0x58--0x00 0x59--0x00 0x5a--0x09 0x5b--0x07
0x5c--0x07 0x5d--0x0a 0x5e--0x44 0x5f--0x21
0x60--0x22 0x61--0x02 0x62--0x00 0x63--0x00
0x64--0x10 0x65--0x00 0x66--0x00 0x67--0x00
0x68--0x00 0x69--0x00 0x6a--0x00 0x6b--0x00
0x6c--0x00 0x6d--0x00 0x6e--0x20 0x6f--0x00
0x70--0x00 0x71--0x00 0x72--0x00 0x73--0x00
0x74--0x00 0x75--0x00 0x76--0x00 0x77--0x00
0x78--0x00 0x79--0x00 0x7a--0x00 0x7b--0x00
0x7c--0x00 0x7d--0x00 0x7e--0x80 0x7f--0x00
0x80--0x00 0x81--0x00 0x82--0x00 0x83--0x00
0x84--0x00 0x85--0x00 0x86--0x00 0x87--0x00
0x88--0x00 0x89--0x00 0x8a--0x00 0x8b--0x00
0x8c--0x00 0x8d--0x00 0x8e--0x00 0x8f--0x00
0x90--0x00 0x91--0x00 0x92--0x00 0x93--0x00
0x94--0x00 0x95--0x00 0x96--0x00 0x97--0x00
0x98--0x00 0x99--0x00 0x9a--0x00 0x9b--0x00
0x9c--0x00 0x9d--0x00 0x9e--0x00 0x9f--0x00
0xa0--0x00 0xa1--0x00 0xa2--0x00 0xa3--0x00
0xa4--0x00 0xa5--0x00 0xa6--0x00 0xa7--0x00
0xa8--0x00 0xa9--0x00 0xaa--0x00 0xab--0x00
0xac--0x00 0xad--0x00 0xae--0x00 0xaf--0x00
0xb0--0x00 0xb1--0x00 0xb2--0x00 0xb3--0x00
0xb4--0x00 0xb5--0x00 0xb6--0x00 0xb7--0x00
0xb8--0x00 0xb9--0x00 0xba--0x00 0xbb--0x00
0xbc--0x00 0xbd--0x00 0xbe--0x00 0xbf--0x00
0xc0--0x00 0xc1--0x00 0xc2--0x82 0xc3--0x00
0xc4--0x58 0xc5--0x00 0xc6--0x00 0xc7--0x00
0xc8--0x40 0xc9--0x00 0xca--0x00 0xcb--0x00
0xcc--0x00 0xcd--0x02 0xce--0xff 0xcf--0x00
0xd0--0x00 0xd1--0x00 0xd2--0x00 0xd3--0x00
0xd4--0x00 0xd5--0x00 0xd6--0x00 0xd7--0x00
0xd8--0x00 0xd9--0x00 0xda--0x00 0xdb--0x00
0xdc--0x00 0xdd--0x00 0xde--0x00 0xdf--0x00
0xe0--0x00 0xe1--0x00 0xe2--0x82 0xe3--0x00
0xe4--0x48 0xe5--0x08 0xe6--0x00 0xe7--0x00
0xe8--0x00 0xe9--0x00 0xea--0x00 0xeb--0x00
0xec--0x00 0xed--0x02 0xee--0x00 0xef--0x00
0xf0--0x5f 0xf1--0x55 0xf2--0x42 0xf3--0x39
0xf4--0x34 0xf5--0x31

    The GENERAL_STS Register (Address = Ch) is 0x07 . which is not correct.

FOR LCD1

    The dump of the DS90UH941AS  is as follows:

0x00--0x34 0x01--0x00 0x02--0x00 0x03--0x9a
0x04--0x00 0x05--0x00 0x06--0x58 0x07--0x00
0x08--0x00 0x09--0x01 0x0a--0xc1 0x0b--0x00
0x0c--0x16 0x0d--0x35 0x0e--0x33 0x0f--0x03
0x10--0x33 0x11--0x00 0x12--0x00 0x13--0xdf
0x14--0x00 0x15--0x00 0x16--0xfe 0x17--0x1e
0x18--0x7f 0x19--0x7f 0x1a--0x01 0x1b--0x00
0x1c--0x00 0x1d--0x00 0x1e--0x01 0x1f--0x00
0x20--0x83 0x21--0x00 0x22--0x25 0x23--0x00
0x24--0x00 0x25--0x00 0x26--0x00 0x27--0x00
0x28--0x01 0x29--0x20 0x2a--0x20 0x2b--0xa0
0x2c--0x00 0x2d--0x00 0x2e--0xa5 0x2f--0x5a
0x30--0x00 0x31--0x09 0x32--0x00 0x33--0x05
0x34--0x0c 0x35--0x00 0x36--0x00 0x37--0x00
0x38--0x00 0x39--0x00 0x3a--0x00 0x3b--0x00
0x3c--0x00 0x3d--0x00 0x3e--0x81 0x3f--0x02
0x40--0x08 0x41--0x05 0x42--0x20 0x43--0x00
0x44--0x00 0x45--0x00 0x46--0x00 0x47--0x00
0x48--0x00 0x49--0x00 0x4a--0x00 0x4b--0x00
0x4c--0x00 0x4d--0x00 0x4e--0x00 0x4f--0x8c
0x50--0x16 0x51--0x00 0x52--0x00 0x53--0x00
0x54--0x02 0x55--0x10 0x56--0x01 0x57--0x02
0x58--0x00 0x59--0x00 0x5a--0x09 0x5b--0x01
0x5c--0x02 0x5d--0x0a 0x5e--0x44 0x5f--0x64
0x60--0x22 0x61--0x02 0x62--0x00 0x63--0x00
0x64--0x10 0x65--0x00 0x66--0x00 0x67--0x00
0x68--0x00 0x69--0x00 0x6a--0x00 0x6b--0x00
0x6c--0x00 0x6d--0x00 0x6e--0x20 0x6f--0x00
0x70--0x48 0x71--0x00 0x72--0x00 0x73--0x00
0x74--0x00 0x75--0x00 0x76--0x00 0x77--0x48
0x78--0x00 0x79--0x00 0x7a--0x00 0x7b--0x00
0x7c--0x00 0x7d--0x00 0x7e--0x77 0x7f--0x00
0x80--0x00 0x81--0x00 0x82--0x00 0x83--0x00
0x84--0x00 0x85--0x00 0x86--0x00 0x87--0x00
0x88--0x00 0x89--0x00 0x8a--0x00 0x8b--0x00
0x8c--0x00 0x8d--0x00 0x8e--0x00 0x8f--0x00
0x90--0x00 0x91--0x00 0x92--0x00 0x93--0x00
0x94--0x00 0x95--0x00 0x96--0x00 0x97--0x00
0x98--0x00 0x99--0x00 0x9a--0x00 0x9b--0x00
0x9c--0x00 0x9d--0x00 0x9e--0x00 0x9f--0x00
0xa0--0x00 0xa1--0x00 0xa2--0x00 0xa3--0x00
0xa4--0x00 0xa5--0x00 0xa6--0x00 0xa7--0x00
0xa8--0x00 0xa9--0x00 0xaa--0x00 0xab--0x00
0xac--0x00 0xad--0x00 0xae--0x00 0xaf--0x00
0xb0--0x00 0xb1--0x00 0xb2--0x00 0xb3--0x00
0xb4--0x00 0xb5--0x00 0xb6--0x00 0xb7--0x00
0xb8--0x00 0xb9--0x00 0xba--0x00 0xbb--0x00
0xbc--0x00 0xbd--0x00 0xbe--0x00 0xbf--0x00
0xc0--0x00 0xc1--0x00 0xc2--0x82 0xc3--0x00
0xc4--0x50 0xc5--0x00 0xc6--0x00 0xc7--0x00
0xc8--0x40 0xc9--0x00 0xca--0x00 0xcb--0x00
0xcc--0x00 0xcd--0x02 0xce--0xff 0xcf--0x00
0xd0--0x00 0xd1--0x00 0xd2--0x00 0xd3--0x00
0xd4--0x00 0xd5--0x00 0xd6--0x00 0xd7--0x00
0xd8--0x00 0xd9--0x00 0xda--0x00 0xdb--0x00
0xdc--0x00 0xdd--0x00 0xde--0x00 0xdf--0x00
0xe0--0x00 0xe1--0x00 0xe2--0x82 0xe3--0x00
0xe4--0x40 0xe5--0x08 0xe6--0x00 0xe7--0x00
0xe8--0x00 0xe9--0x00 0xea--0x00 0xeb--0x00
0xec--0x00 0xed--0x02 0xee--0x00 0xef--0x00
0xf0--0x5f 0xf1--0x55 0xf2--0x42 0xf3--0x39
0xf4--0x34 0xf5--0x31

     The GENERAL_STS Register (Address = Ch) is 0x16 . which is also not correct.

   The situation is .

   i can get the i2c address of the DS90UH948 from the DES_ID_DES_ID_1 Register (Address = 6h) .which is 0x58. like it's shown in the register dump:

0x06--0x58 

  but i'm not really able to access the remote i2c address of DS90UH948 .

 

FPD-Link III is generated from external oscillator provided to REFCLK pin with a 100MHz input.

The fpdlink cable is twisted pair cabling

     

     My question is:

   what might be the reason for such fpdlink setup failure?

   what are the neccessary steps (hardware/software) to get the fpdlink correct setup?