Part Number: DS90UB934-Q1EVM
Other Parts Discussed in Thread: ALP, DS90UB933-Q1, , USB2ANY
Hello,
This is Ahmed embedded software engineer at Valeo,
I am working on DS90UB934-Q1EVM Evaluation kit (deserializer) and DS90UB933-Q1 (serializer) using ALP software that is downloaded from link :
when i connect the deserializer to the PC using the micro USB, PC is not able to recognize the deserializer and considered it as unknown.
we tried to use another deserializer kit but it gives same behavior.
I powered the deserializer kit with 12v in J26 and it draws around 260 m Amps,
Camera is powered by 9v, it draws 107 m Amps
I really appreciate if we can arrange for a quick call make it easier and clearer.