Part Number: PCA9543A
Other Parts Discussed in Thread: TS5A23159, TS5A23157
Hi,
PCA9543A is 2 channel I2C bidirectional switch. Can I use the same for MDC/MDIO switching.
The requirement is MDC & MDIO interface should go to devices with same MDIO address. So, we need a switch to differentiate the different devices. The required BW of MDC/MDIO is 2.5MHz and voltage supported is 1.8V, but PCA9543A supports only frequencies upto 400KHz and voltage 2.3 to 5.5V.
Please suggest an alternate part if this part is not suitable for our requirement.
Thanks,
Tejaswi