Part Number: TUSB9261
I am Designing a carrier board for an SOM
I need Usb 3.0 to Sata Brigde Embedded.
Is the SPI Flash and Jtag Connector Nessesary?
Can I design TUSB9261 without SPI Flash and Jtag Header.
Will it work?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We do have a old tool I can share however wo do not currently support this tool. It has also been reported that it does not compile on recent versions of Linux due to deprecated dependencies. If you are very familiar with Linux you may be able to modify and get it working on your platform but I will not be able to provide help here.
Otherwise I suggest creating a complete FW image though the flashburner tool using a windows machine. Using this tool you can read beck the complete contents of the SPI flash then externally program your onboard SPI flash so that TUSB9261 may load the FW correctly.