Part Number: DP83867E
Hello team,
I received a question from the customer about PHY extended setting "Robust Auto-MDIX" of DP83867. I would appreciate if you could give us a advice about it.
In checking the link operation of PHY (DP83867), it was confirmed that it did not work properly. As a result of the investigation, it was confirmed that this problem can be solved by enabling the extended setting "Robust Auto-MDIX" of the PHY. The PHY data sheet does not state that it is mandatory to enable "Robust Auto-MDIX".
Could you give us feedback on the impact of implementing this setting?
■ Occurrence phenomenon (case where a problem occurs)
DP83867 link setting: fixed at 100 Mbps
Link setting on the opposite side: Auto-negotiation
If you connect to each other (*), the phenomenon like "link up does not occur" or "it takes several minutes to link up" occurs.
* This connection form is not a preferable connection form, but at least it should link up.
Best Regards,
Ryotaro Fukui