Part Number: SN75DP159
Hello team,
I have a question about SN75DP159's recommended capacitors value for VDD pin and VCC pin.
Datasheet fig30-33 have 4 x 0.1uF, 2 x 0.01uF and 1 x 10uF for VDD pin.
However schematic checklist(slla461) says 5 x 0.1uF, 1 x 4.7pF, 1 x 10pF and 1 x bulk cap and there is slight difference from datasheet.
Same as above, there is difference for also VCC pin.
Which datasheet or checklist is better? or please let me know if there is other combination which is better than the two.
Best regards,