Part Number: TPS25750
Other Parts Discussed in Thread: BQ25731,
We're using the TPS25750 as a DRP with the BQ25731. When used as a source the load has a large current spike at the beginning, then tapers down to the expected 60-100W.
During the large current spike we see the VBUS and PP_HV voltage get pulled pretty low for ~4ms (from 20V to 15V or even 10V). This causes the circuit to turn off, I'm not sure if it's because of over current (we have the TPS25750 to allow a 200% over current) or under voltage. In any case is there a way to program the TPS25750 to automatically turn back on? Other USB-C supplies we've tested also drop out but then come right back on. Just wondering if there is a setting in the TPS25750 that allows this?
The USB-C device we are powering sometimes has some residual voltage on VBUS (~1-3V). This seems to prevent the TPS25750 from negotiating with the device (it does work once the voltage drops below 1V). Other supplies we've tested don't seem to have this limitation. Is there a way to set the TPS25750 to tolerate this condition?
Thanks,
Nick