Part Number: MAX3232E
MAX3232E has recommended VCC specs of 3.3V +/- 0.3V or 5.0V +/-0.5V. First page of data sheet indicates, "Operates with 3V to 5.5V VCC Supply".
Any issue operating this part at VCC = 4.4V? (This is a diode drop below 5V). It seems like it would be just fine, but the recommended specs are oddly specific to the ranges listed.
Thanks, Best, Steve