This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX232: Are these possible to use charge pump capacitor(C1-C4) is 2.2uF

Part Number: MAX232

Dear Specialists,

My customer is considering MAX232ID and has a question.

I would be grateful if you could advise.

---

According to the datasheet, charge pump capacitor(C1 to C4) should use 1.0uF of ceramic, Tantalum or electrolytic.

Are these possible to use ceramic 2.2uF instead of 1.0uF

When possible, what should it be aware of. 

--

I appreciate your great help in advance.

Best regards,

Shinichi