Part Number: DS90UB960-Q1
Other Parts Discussed in Thread: ALP
Hi,
I'm using PSDKR v7.2, and want to read registers from UB960/UB953, but cann't find such APIs in source of imaging component.
I know I can implement them by myself and I've done these actually. But they should be implemented officially.
If there are APIs for writting, then APIs for reading should be implemented too.
And sometime uses may want to log registers in their code for debugging.
And I know I can use ALP GUI to read registers, but according to above reasons, please don't guide me to ALP GUI.
BTW, ALP GUI v1.57.0010 influence test result : our back channel frequence back to 50M when I just open it without any other operation.