Part Number: TPS65987EVM
Other Parts Discussed in Thread: TPS65987D
Hi Team,
I got TPS65987EVM and did the same content of "3.2 Application Configuration GPIO Event Settings" in page 7.
https://www.tij.co.jp/jp/lit/an/slvae11a/slvae11a.pdf
As a result, I found there is opposite transition of GPIO in the application note referred.
------------------------------------------
(wrong)
The example shows that TPS65987D transmit new source capabilities 5 V, 3 A when GPIO4 goes from high to low
and 5 V, 3 A and 9 V minimum 20 V maximum, 3 A when GPIO4 goes from low to high.
(correct: actual function)
The example shows that TPS65987D transmit new source capabilities 5 V, 3 A when GPIO4 goes from low to high
and 5 V, 3 A and 9 V minimum 20 V maximum, 3 A when GPIO4 goes from high to low.
------------------------------------------
So, I believe the following red part is opposite (typo) in GUI.
Could you look into it?
Best Regards,
Yaita