Part Number: TFP401A
Hello,
Regarding to setup/hold time on TFP401A,my customer is asking some question.
Their configuration: 1 pixel/clock, PIXS = low, OCK_INV = high, fODCK=65MHz
(Question)
1) According to datasheet page 8, set time(minimum ) and hold time(minimum ) are 2.1(ns)/0.5(ns).

Are these values at fODCK=165MHz?
If so, do you have some data(min/typical/max) of 65MHz?
From below thread, setup time is 4.5ns and hold time is 10ns at 65MHZ. Are these values typical?
If so, do you have some data(min/max) of 65MHz?
2)They think about estimating of set time(max) and hold time(max) as following.
t_su2(max)=1/freqency - t_h2(min)
t_t2(max)=1/freqency - t_su2(min)
fODCK=65MHz
t_su2(max)=15.38ns - 0.5 = 15.33ns
t_t2(max)=15.38ns - 2.1 = 13.28ns
Their understanding is correct?
Regards,
Tao_2199