Part Number: DP83822I
Hello,
Can I use "INT/PWDN" pin of the PHY DP83822I as output for "Link Status" ?
i.e.:
INT/PWDN (Pin 8) = "Low" (0V) --- for Link Down
INT/PWDN (Pin 8) = "High" (3.3V) --- for Link Up
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83822I
Hello,
Can I use "INT/PWDN" pin of the PHY DP83822I as output for "Link Status" ?
i.e.:
INT/PWDN (Pin 8) = "Low" (0V) --- for Link Down
INT/PWDN (Pin 8) = "High" (3.3V) --- for Link Up
Hi Rohidas,
"INT/PWDN" pin cannot be used as output for link status. I recommend using "LED_0" pin for link status.
Regards,
Adrian Kam