Part Number: DS90UB960-Q1
Dear team,
My customer uses 960 paired with 4*935 in the SVS project. They use interleave mode because SOC doesn't have enough VC channel. They also use internal frame sync signal to sync four cameras. Currently they encounter a problem. When one camera is remove while other three cameras are still connected, the remained three cameras can't work normally, and there is no image displayed.
If they change interleave mode to round robin mode, the remained three cameras can work normally even though one camera is disconnected.
Could you please help analyze what the root cause is, the interleave mode, or SOC software?
If the root cause is interleave mode, is there any solution to solve this issue?
Thanks & Best Regards,
Sherry