Part Number: TUSB9261
For TUSB9261, is the default firmware pre-loaded?
Or, do I need to load the firmware via SPI Flash before use?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB9261
For TUSB9261, is the default firmware pre-loaded?
Or, do I need to load the firmware via SPI Flash before use?
Hi,
TUSB9261 does not have FW pre-loaded Boot code will only perform a burst read to the connected SPI flash. The connected SPI flash should be pre-programmed with complete FW image or programmed on-board with the flashbuner SW found on ti.com (windows OS only). The TUB921 flashburner creates the complete FW image that should be used for program the SPI Flash.
Hi,
TUSB9261 does not have FW pre-loaded Boot code will only perform a burst read to the connected SPI flash. The connected SPI flash should be pre-programmed with complete FW image or programmed on-board with the flashbuner SW found on ti.com (windows OS only). The TUB921 flashburner creates the complete FW image that should be used for program the SPI Flash.
Hi,
TUSB9261 does not have FW pre-loaded Boot code will only perform a burst read to the connected SPI flash. The connected SPI flash should be pre-programmed with complete FW image or programmed on-board with the flashbuner SW found on ti.com (windows OS only). The TUB921 flashburner creates the complete FW image that should be used for program the SPI Flash.