Part Number: TPS25814
Dear Team,
My customer is considering to use the TPS25814 with standalone mode, so the following pins are not used.
Please check setting of each unused pin.
- /POL --> Can be left open, or can be connected to GND
- /SINK --> Can be left open, or can be connected to GND
- /DEBUG --> Can be left open, or can be connected to GND
- I2C_EC_SDA --> Tie to pullup voltage (LDO_3V3) through a pullup resistor 2.2kohm
- I2C_EC_SCL --> Tie to pullup voltage (LDO_3V3) through a pullup resistor 2.2kohm
- I2C_EC_IRQ --> Tie to pullup voltage (LDO_3V3) through a pullup resistor 10kohm, or other?
Thank you.
Best Regards,
Koshi Ninomiya