Part Number: TUSB4041I
Tusb4041ievm 3.3V and 1.1V power supply both use 1A power chip, but my actual application load power consumption is only tens of Ma. Through calculation, I use 300mA power chip to supply 3.3V power and the same chip to supply 1.1V power. However, the computer can identify hub but not USB device, but the test overall power consumption is about 200mA. Please help to analyze the power consumption problem?