This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4041I: Abnormal connection

Part Number: TUSB4041I

Tusb4041ievm 3.3V and 1.1V power supply both use 1A power chip, but my actual application load power consumption is only tens of Ma. Through calculation, I use Digital voltage source power supply 3.3V&1.1V,current output capacity of more than 1A,However, the computer can identify hub but not USB device, Attached is the schematic diagram and PCB, please help to analyze the reasons 。

TUSB4041-TEST.pdf

TUSB4041(1).pdf