Part Number: DP83822H
Hi,
my customer has the following question regarding the linking of the DP83822H:
Within the scope of the EtherNet/IP certification it is necessary that the link can be firmly configured. As a minimum, the device must support autonegotiation, 100Mbit-FD and 10Mbit-FD. Now the remote station is left on autonegotiation during the test and it is expected that the link is established and the device is reachable, but this is not the case. Only after I change the configuration of the network interface on the PC and set it to a predefined speed, the link is established and the device is accessible again.
In the past they have used the phys and switches of a competitor. These have also established the link to the PC with a fixed link speed and deactivated autonegotiation. Can you set this in DP83822H Phy as well?