Part Number: DP83826I
Other Parts Discussed in Thread: DP83826EVM
Hello,
I can't make the DP83826I stablish link with this schematic: (If I remove the choke and the transformer and place 4x 33nF capacitors in-line it works perfectly, so the issue is with the magnetics)
The transformer PN is: Wurth 74930000 and the common mode choke PN is: Wurth 744232222.
I've tried removing the choke, adding more capacitance to the CT, trying different discrete transformers... I've also tried it in multiple boards, so it's not a soldering issue...
Can someone help me seeing what's wrong here?
Thanks in advance,