This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: Unplugging and Plugging back in to charge

Part Number: TPS65987D


I have a custom board with the TPS65987D that is referenced to the EVM, that I am supplying power to the board, similar to the EVM (i.e.:10 to 20V).

When it comes to charging the device, if the phone is plugged into the the USB-C cable to the USB-C on the board and 20V is then applied to the board. I have to disconnect the USB-C and reconnect to get the phone to charge.

Is there setting that can be changed to fix this?

Thanks in advance