Part Number: TPS65987D
I have a custom board with the TPS65987D that is referenced to the EVM, that I am supplying power to the board, similar to the EVM (i.e.:10 to 20V).
When it comes to charging the device, if the phone is plugged into the the USB-C cable to the USB-C on the board and 20V is then applied to the board. I have to disconnect the USB-C and reconnect to get the phone to charge.
Is there setting that can be changed to fix this?
Thanks in advance