Part Number: TPS65987D
Other Parts Discussed in Thread: TUSB8042A, LM3489
Hello,
I have a custom board where I am using the TPS65987D in various power paths and have had little success.
I am trying to use it as a DRP device, where I can either:
1. Connect VBUS through a USB-C to a phone, to supply 5V out on PPHV1 to my system power.
2. or while VBUS is connected through USB-C to a phone and if I supply 10-20V, the TPS65987D would switch from supplying power through PPHV1 from the phone and will source VAR_DCDC (5V, 9V, 15V, 20V @ 3A), like shown in the EVM and charge the phone, through PPHV2 path to VBUS.
3. And then switch back to supplying 5V out on PPHV1 if I disconnect the 10-20V input
All while maintaining my connection to the upstream side of my USB Hub TUSB8042A
I am also using the FT4232H Mini Module to flash the device, same IC from the EVM used to flash the PD, I have had some success flashing the memory occasionally through SPI Flash.
Any suggestions or configuration binary file that could be provided would be greatly appreciated.