This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB320: Please help to achieve Power Delivery (up to 100W) Solution together with TUSB320 (in DRP data mode)

Part Number: TUSB320

Dear Team,

We are building a system which have USB Type C connector, Power Delivery capability of up to 100W and TUSB320 chip for interfacing with USB 2.0 OTG Peripheral Unit on our SoC (it has ID pin). We need Power Delivery to be operable at DRP mode of TUSB320. Please advice answers on the following questions:

1. Can we connect together by hardware pins CC1/CC2 lines of TUSB320 and some PD controller chip?

2. Could you advice some PD controller chip which can work together with TUSB320 (at least 30W, 100W will be just fine. TUSB320 will operate in DRP only.)

3. Could you advice some app note/document which describes schematics of such or similar solutions?

Thank You,

Sergey