This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS160PR822: Use in I2C slave mode for PCIe applications?

Part Number: DS160PR822
Other Parts Discussed in Thread: DS160PR810

We are considering to use a handful of the DS160PR822 devices in a PCIe application.

The datasheet says: "The device is in normal operation with PCIe state machine enabled by RX_DET = L1/L2/L3". However this is a shared pin: RX_DET / SCL. For operation in I2C mode, SCL must have a pull-up. L1 and L2 requires pull-down and L3 requires an 'open'. Is it possible to enable the PCIe state machine with the RX_DET / SCL pin connected to an I2C bus?

Terje