Part Number: DP83869HM
Hi.
I was confused about the description of ANA_RGMII_DLL_CTRL Register (address 0x86).
I need to confirm the following questions:
(1) Is the clock-shift value ignored if it is set to aligned mode in RGMII_CTRL Register (Address = 0x32)?
(2) Is it a MUST to set bit[8] to 1 that shift values take into effect? I found it seems that TX-shift value takes into effect only when bit[8] is set to 1.
(3) What is the meaning of DLL_EN_FORCE_VAL, bit[9] of ANA_RGMII_DLL_CTRL Register? And how to set it?
Thanks.