This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75LVCP601: Is SN75LVCP601 supports SATA3 or SATA2 only

Part Number: SN75LVCP601


Hi,

When "quick search" for the SATA3 redriver, the SN75LVCP601 is not a matching part.

If I lower the protocol to SATA2 redriver, the SN75LVCP601 is seen as an option.

https://www.ti.com/interface/pcie-sas-sata/products.html#p1241=Redriver;Retimer&p2094=SATA&p1389=SATA2

vs

https://www.ti.com/interface/pcie-sas-sata/products.html#p1241=Redriver;Retimer&p2094=SATA&p1389=SATA3

But at the same time, the SN75LVCP601 is for up to 6Gbps interfaces.

Any reason why it wouldn't be part of the "SATA3" protocol ?

Thanks,

Luc