Part Number: THVD8000
Other Parts Discussed in Thread: THVD8010
Hello everyone!
I'm glad to be able to use the THVD8000 chip, our team absolutely love it.
But I can't understand how to calculate the inductance correctly for THVD8000 / THVD8010 chips.
I need transmit data via the power line (about 20 meters of non-twisted cable, AWG14) at low speed (9600 b/s is enough for me) between two devices. At the same time, a large current sometimes flows along the line, 12 volts 5 amperes.
Initially I planned to use the minimum frequency of 125 kHz. However, when calculating the inductances, a very large value is obtained. Inductors of this rating with a current of 5a or more take up a lot of space on the board, and I simply cannot place them, they will not fit.
What are the disadvantages when choosing a frequency for example 1 MHz or 5 MHz? I am thinking to choose 5 MHz.
And I cannot understand the datasheet corrrectly: how to calculate the inductance correctly.
L = 750 / (2 * 3.15 * 5) = 24 uH
I choose a frequency, look at the graph.
1) Will I get the total inductance of the two coils or the inductance of each of them?
For example, for a frequency of 5 MHz, should I use two chokes at 48 μH or two at 24 μH (on the each side)?
2) I don't understand what this phrase means:
If no termination is used in theapplication, then the total equivalent impedance at the carrier frequency could be reduced to Z ≥ 60 Ω
3) How can I lower the inductance requirements?
Thanks!