This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB921-Q1: coax support deserializer pair

Part Number: DS90UB921-Q1


Hi, 

I have seen some posts recommending to use the 926 in place of the 922 when paired with the 921 serializer. I have a use case where we need to use coax and not twisted pair. Can you suggest which deserializer i would need for this case as it is not clear to me from the datasheet and parametric table if the deserializer can support this. The deserializer would need to output RGB888, VS, HS, and DE as parallel data.

Thanks, 

Jose