Part Number: DS90UB960-Q1
I have a custom PCB with a 960 device. I have one of the ports connected to a 953 serializer and I am running in CSI-2 mode.My problem is that I cant get a consistent lock. If I read register 0x4d every 0.5s then I get the following values 0x70, 0x50, 0x53, but mostly 0x50. It seems that it is locking at times. I originally had about 2m of coax cable but I have shorted it to about 2cm but it made no difference. Are there any registers that I need to set before it will lock consistently? I originally had the design working on the 960 eval board, But I was using the Analog LaunchPAD software. I'm not sure if that was setting other registers by default.