Part Number: TPS65987D
Hi, team,
Let me check the Dead battery operation of TPS65987D.
In the hardware I am designing, SPI Flash (FW and initial settings) is connected to TPS65987D, and control is performed from the microcomputer connected via I2C1.
Also, I am thinking of setting "BP_NoResponse, Safe" in the hard strap setting of ADCIN1.
At this time, when VIN_3V3 is 0V, if the connection partner has Source capability, VBUS is output from the other party and 3.3V is output to LDO_3V3.
(Q1) If LDO_3V3 is started by VBUS when VIN_3V3 is 0V and then VIN_3V3 becomes 3.3V, what is the timing when FW and settings are read from SPI Flash?
From the description in "Table 6" of "SLVSES1B", I think that reading starts after VIN_3V3 becomes 3.3V. Is this correct?
(Q2) Is it possible to control by communicating with TPS65987D with I2C1 after VIN_3V3 becomes 3.3V?
(Q3) Isn't it possible to see the voltage from the VBUS terminal to PP_HV1 and PP_HV2 before instructing the VBUS terminal and PP_HV terminal to turn on the switch by I2C1 control?
Best regards,
Hamada