Other Parts Discussed in Thread: SN65DSI84
Customers need one Mipi input and two LVDS outputs, holding 1920 × 1200 × 24 @ 60fps? What is recommended?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN65DSI84
Customers need one Mipi input and two LVDS outputs, holding 1920 × 1200 × 24 @ 60fps? What is recommended?
Hi Kevin,
Customer can check the SN65DSI84. However, please check the supported LVDS clock frequencies on the display panel datasheets. 1920x1200 @60Hz is right at the edge of the SN65DSI84's max supported LVDS clock frequency of 154 MHz.
Regards,
I.K.