Part Number: ONET1141L
Hi Everybody
I have questions.
1. If I use data input DIN+ with 0 ~ 2.0V only (don't use DIN-). And then do I have to float DIN-? or connect to GND?
2. If I use data input as question 1, ONET1141 driver laser well?
3. DIN impedence is 100 Ohm. If I use 50 Ohm input, then I have to connect 100 Ohm resistor at DIN?