Part Number: TPS65987DDJ
Other Parts Discussed in Thread: TPS65987D
Hi ti Team,
Further review to the type C Block diagram, I have a new comment please review if it is possible to implement.
1,USB audio is a default setting for the system, play back for 192K/96K/88.2K/48K/44.1K sampling USB audio signal, since it is an important feature of the product, I would like to exchange USB audio chip D+,D- signal with the USB type C controller as illustrated by below photo, the USB audio D+,D- only need to go through an USB switch but not two switchs to maintain high quality RF signal .is there any issues for D+,D- signal deom USB type C connector to USB controller chip via two switchs?
2,Need to support BC1.2 please confirm.