This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: how to set pixel clock

Part Number: DS90UB954-Q1

Hi team,

You mention 'FPD3_PCLK = 2 × fCLKIN or 1 x fCLKIN' at datasheet p.29.

Could you teach me which should I choose? 

And could you teach the flow to choose?

*Following is copy of datasheet.

Best regards,

Takao

  • Hello Takao,

    this depends on the value of the used External Clock connected to the SER. If the CLK value is between 25-52MHz then you multiply by 2. But if the CLK value is between 50 - 104MHz, then you multiply by 1.

    Please refer to Table 7-6 in the 953 datasheet.