TI's AN-1509 detailed several configurations of PHYterDual port switching, including one where port A and B acted as a repeater, but the RX data from each port was also mirrored to the MAC over MII/RMII. This is a very useful feature, and even though TI's Gigabit Ethernet PHYs don't come in a dual package, I was hopeful I could pull it off. Rod Rodrigues responses in the thread below about using the DP83867 back to back made me wonder if I could accomplish the desired repeater with port mirroring function for Gigabit Ethernet.
(+) Back to back Gigabit Ethernet Phys??? - Interface forum - Interface - TI E2E support forums
Would it work to tie in an RGMII MAC to the RX lines for each port? to accomplish this? (see image from AN-1509 pg 8 below)