This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB934-Q1: Questions for Compatibility

Part Number: DS90UB934-Q1
Other Parts Discussed in Thread: DS90UB914A-Q1,

Hello, Team,

Our customer wants to double-check two things:

  1. Is DS90UB934-Q1 p2p compatible with DS90UB914A-Q1?
  2. Are there any issue with connecting DS90UB913x-Q1 with DS90UB934-Q1?

For 1, it would be ok to replace UB914 with UB934 since it is stated as an improved version of UB914 in the datasheet.
They want to double check because the package is different, and some of the pin names are different as well.
For 2, it should be no issue since it is a connection of FPD-LINKs.

Thanks and Best Regards,
Masaru Oinaga