Part Number: TUSB320HAI
Other Parts Discussed in Thread: TPD8S300
Hi Team,
My customer using TUSB320HAI and they encounter the ESD issues on CC1 and CC2. They would like to pass ESD conditions are contact ±6kV , air ±15kV that is their customer criteria also. However, they did the 3 approaches on the CC1 and CC2 but still got the failure on +4KV.Note: 3 approaches they did as the following:
- Adding varistor (5.5V,10pF, TVM0G5R5M100R)
- Adding 5V TVS
- Adding a resistor(9.1ohm) in series.
Could you kindly provide what the ESD components or other suggestion that can improve ESD ability on CC1 and CC2.