Part Number: TUSB322I
Hi Expert,
Customer used TUSB322I and have some questions would like to clarify.
1. INT_N(pin6) is 1.8V, R925 is open, not mounted. When there is a device attached, INT_N would pull low(0V), but when device is detached, why INT_N didn't go back to high, still hold in low? Customer also checked ID pin, and it would change.
2. when device is attached, REG09 = 0x70; when device is detached, REG09 = 0x20.
But why REG08 is always 0x00 not matter device is attached or detached?

Thanks,
Allan