Part Number: DS90CR288A
Hello Team,
My customer is looking for the maximum continuous/pulsed current on the CMOS outputs for safe operations for the DS90CR288A. Do we have this information?
Their application is they need to connect the 3.3 V CMOS outputs to a SoC with 1.2 V CMOS levels. Because of the large number of outputs, level translators seem to be infeasibly, and voltage dividers seem to be a good solution. Now they need to find a good tradeoff for the voltage divider: If the resistances are too high, less current is required but parasitic capacitances will break the signal down. So basically the question is, how low can we go on the voltage divider without damaging the IC by drawing too much current?
Regards,
Renan