Part Number: TPS25750EVM
Other Parts Discussed in Thread: TPS25750
Hi,
I recently acquired the TPS25750EMV evaluation board for the TPS25750 PD controller.
I can connect it to the GUI fine (COM port detected and opened) but when I finish to fill the form and press the "Flash to Device from current configuration" button, the progress bar for the EEPROM stays forever at 0% ("Erasing EEPROM").
Did I miss something ?
The jumpers are all in place (straight out of the box). The EVM is powered with a 20V supply as required.
Thanks for your help.
Best regards,
Marc