Part Number: TUSB320EVM
Other Parts Discussed in Thread: TUSB320, TUSB320LAI
I have my EVM dip switches set such that pin 1, EN# is ON, and pin 7 PORT_H is ON (DFP). I have the micro-B going back to the US port of a USB hub dev kit. Now obviously, the hub US port isn't going to provide the power and this is DFP mode so I don't expect it to just work. And indeed when I plug a phone in when in this mode, I see weird behavior (ID light and power going on and off), probably phone trying to charge and get nothing. That seems normal, time to plug the barrel jack in. I connect it to a benchtop supply and provide around 5.5-6V and see the phone now draw a standard 500mA. But there is no data, it won't get the connection back to the hub and receive the DS ports.
If I turn EN# OFF, I do then get data (devices on hub DS ports)- but no power of course.
If I run in DRP mode (set PORT_H OFF), with NO external power, then I get data (devices on DS ports on my hub). But as soon as I add external power, data is gone same as DFP mode.
D8 is populated and D9 is NOT populated.
Am I doing something wrong or missing some detail? Do I have a defective board?