Other Parts Discussed in Thread: MSP430F5438, TUSB3410
i hav connected the same circuit as in the uartpdk evm and then programmed the eeprom with the tusb3410 eeprom burner utility with the same vid pid as the evm i.e. VID_0451&PID_341A now after programming the eeprom when i connect it to windows 7 32 bit using hyperterminal it says that "unable to open com port . please check settings" and the device disconnects and connects itself to usb again . i hav used the default driver for vcp provided in swrc094f . also on windows xp 32bit and still having the same problem and even on windows 7 64bit . i need to connect it to msp430f5438 for basic uart communication
please help
thanks
Karanpreet Singh