Part Number: TCA6424A
Dear TI Team
Our customers have asked the following questions about the VCCI, VCCP, and RESET pins, so please let us know.
1. Is it okay to connect the power supplies to the VCCI and VCCP pins directly without separating them?
2. If 3.3V is applied to the RESET pin before raising the voltage of the VCCI and VCCP pins, is there a problem in operation?
(If you check the rating of the input voltage, it is 6.5V at the maximum, so I think that it will not be damaged.)
3. As shown in the figure below, is there any problem if the following procedure is performed at startup?
(I think that RESET should be set to High after starting VCCI and VCCP.)
3.3V can be applied to VCCI
→ Release RESET (Set to High)
→ 3.3V can be applied to Vccp
→ Set only Vccp to 0V

Best Regards,
Y.Ottey