Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987, TPS65988
Hi Team,
One of our customer using TPS65987DDH in their design. Having some issues and need some help. Can you please provide some insight on the following:
1. We use I2C port 2 (I2C2). We can only communicate using address 0x20 which contradicts the datasheet. Address 0x38 does not work for us on port 2.
2. In "Hardware Design Guideline for TPS65987" (slva888c) table 1-1 indicates that port I2C1 should be connected to a microcontroller rather than port I2C2. Would you recommend I change the design to I2C1? What are the implications of using I2C2? Is this related to the address issue?
3. What is the best way to determine that the PD controller has fully booted? We run into a start up issue where the MCU tries to communicate with the TPS65987 before it is ready when booting off of the internal battery.
4. Attached is the schematic and pjt file. We are using application tool v6.1.1 Can you help to check if there is any wrong settings that might be related to the I2C2 address issue we observed?
Look forward to your feedback. Thanks in advance.
TPS65987DDH_sink_highest_power_v4.pjt
Thanks and regards,
Don