Part Number: TUSB2046B
Other Parts Discussed in Thread: TPS2042
Dear Forum
The sole purpose of my application for TUSB2046 is to make a connected USB-device boot-up by emulating a USB-host. There will be NO DATA COMMUNICATION.
The USB-device is externally powered.
This kind of behavior was previously confirmed with random off the shelf USB-hubs that were powered without connecting them to a USB-host PC.
Assuming that this behavior would be reproducible with ANY USB-hub, I designed the following circuit based on TUSB2046B.

The behavior that I now observe is somehow unexpected. In a few words - the USB-device only starts booting-up when the hub is or was connected to a USB-host.
I have tried to depict the sequence and behavior for a clear understanding.
The circled numbers indicate the sequence of connecting/disconnecting the respective wire


It remains unclear, why the device would not boot-up when the hub is not connected to the USB-host?
If this cannot be answered - how can I emulate a USB-host to the hub (the application will have no access/connection to a PC)
I hope that I was able to describe the issue that I am facing in a clear and consistent manner and that someone out there comes up with a hint or even a solution.